Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Double Clip

Double Clip
Sales Price: 0.71 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 2
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Temporary filing of documents
5
From Japan
On 2019-02-07 14:49:35
If it is about 10 sheets, it will be a rough guide when putting together documents with a sem clip, with 20 or more sheets with a double clip. However, if it is about 20 sheets, it is delicate thickness to clip. Often the thickness of the clip itself gets in the way. However, it is often helpful to organize documents of such subtle thickness, and it is a great help to have a clip of this size. Among similar smaller double clips, it is the easiest to use ever.
This review is about item#48871225.
For office use
4
From Japan
On 2018-08-09 11:06:32
It is an essential item to organize documents. We also purchase clips of different sizes.
This review is about item#48871191.
As a joint part of the cardboard maze.
5
From Japan
On 2015-10-05 16:51:07
I was looking for a big clip, it was good that I could purchase at a low price.
This review is about item#48871173.
Filing of historical materials by age of 50 years memorial development process
4
From Japan
On 2014-01-27 16:51:17
Although it does not feel much when using a small clip, when it is a large clip of 100 class classes, the depth (gripping shila) when closed is large, so it is difficult to maintain in a spread state when it is closed in a binding style , The closed back side is too much overlapping and can not be read. It will be a matter of course, but sometimes I think that something with a short length can be done even if the clip has a wide width (a lot of stitching numbers). When it becomes a big clip, when using it (when opening the clip) strong force is needed and it is difficult to handle with women etc. Naturally, a big clip enters a big clip though. Because it is rare to clip 30 sheets with 150 possible clips, consider only the function of the clip's worker (the gap before use is 0 mm in the case of opening 20 mm to bind for 0 mm) If you start with a state of 10 mm instead of 0 mm for the gap of the state of Mama, I think that we can reduce the force even a little. Of course there will be problems with retention after clipping!
This review is about item#48871173.
1
Customer Who Viewed This Item Also Viewed
Double Clip
Double Clip
Binder Clips
Free label wide
Hazardous substance labeling (iron plate)
Garasushikan bottle
Double Clip
Black Binder Clip