Buy more than* S$200* and get FREE SHIPPING
Note
Due to Japanese national holidays as Golden Week, we will close 2019/4/27~2019/5/6 JST.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Angle Brackets

Angle Brackets
Sales Price: 0.60 SGD
Review Rating: 3.33
3 Customer Reviews
5 star 1
4 star 0
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
When reinforcing the shelf
5
From Japan
On 2017-04-11 09:46:12
It was outside. Although it is inexpensive, I thought that quality is also good, looking beautiful. Sorry it is because there are no indications of inside folding or outside folding. If you hurry, you are in trouble.
This review is about item#58890851.
securing bracket
3
From Japan
On 2016-08-19 13:09:12
Although it is pointed out that the screw hole diameter is not written, is not unnatural to just say Monotaro's answer? Please also include screw hole diameter in answer.
This review is about item#58890772.
Reinforcement and strength improvement of building structural members
2
From Japan
On 2015-12-29 14:33:13
Questions for Specifications Improvement Request Points 1) Please indicate the inner diameter display of the tightening screw hole or the applicable thread diameter in the specification details. (It is difficult to prepare the screw beforehand because the diameter of the screw to be used is unknown.) 2) Tightening hole chamfering direction is unknown, and dissatisfaction remained in this use. This item was for outer tightening, and what I actually wanted was for inner tightening. (In the specification column, you should distinguish between display for outside, inside use etc. If you are going to use both, you should be chamfered on both sides C 05. 3) For this time F-904, What if you set the diameter to 3.2 to 3.5 mm? The wood screw diameter M 3.1 could not be used, it became M 2.7, the driver bit became # 1, a cruciform hole licking occurred, and it was hard for many.
This review is about item#58890815.
1
Customer Who Viewed This Item Also Viewed
Small L Shape Bracket
Square corner
Door Roller Shaft
Stainless Corner Brace
Uniqlo Kanaori Sumikin
Color Gold Fold
UNIQLO two quarters
Habahiro gold folding
Straight Corner Braces
Stay for upper lid
Thick Corner Brace