Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Y Wrench

Y Wrench
Sales Price: 10.99 SGD
Review Rating: 4.00
7 Customer Reviews
5 star 4
4 star 0
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Remove the cover of the drive unit of the moped motorcycle, change the gear oil
5
From Japan
On 2018-05-21 16:01:42
I need an 8 mm, 10 mm wrench and I found this. I was able to work as intended and I was satisfied. I felt that the quality was also good.
This review is about item#60940835.
Maintenance of mopeds
3
From Japan
On 2016-06-04 18:52:59
I use it for parts that I do not want to apply much. Because the accuracy is not good and the outside diameter is also large, there are parts that are not narrow enough to enter.
This review is about item#60940835.
To maintenance of moped
3
From Japan
On 2016-01-15 23:31:50
It was good if it was 8 mm, 10 mm, 12 mm. I do not use 9mm much.
This review is about item#60940835.
Bicycle maintenance work
5
From Japan
On 2015-11-26 17:31:09
It is easy to use with a size that fits in the palm of your hand. In order to use 9 mm for adjustment of the derailleur, together with the other 8 mm and 10 mm, the size to be used most is aligned and it is very good.
This review is about item#60940835.
To maintenance of moped
2
From Japan
On 2015-09-20 10:46:14
I wish it was 8 mm, 10 mm, 12 mm · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · Do you use 9mm? Is it? Is it?
This review is about item#60940835.
As a mobile tool in touring
5
From Japan
On 2015-05-17 16:28:48
It is compact and the best to carry. Durability is not expected because the price is reasonable. I do not think that it will be used so much, so I think it is quite possessive.
This review is about item#60940835.
To the nut fixing the wire of the rear derailleur of the bicycle
5
From Japan
On 2014-06-14 14:49:09
This nut is hard to use with ordinary wrench or plate ratchet. By using this Y type it is possible to fix accurately and quickly. It will not be broken at first, but if you lose it will repeat.
This review is about item#60940835.
1
Customer Who Viewed This Item Also Viewed
Flat Head Screw
YB Y Type Box Wrench
Cross Nut Wrench
6In1 3Way Wrench
3 Way Box Wrench
Y-type socket wrench
Y-type wrench
Cross Rim Wrench
Cross Wrench
Super Horse Band (Naked)
Mini Y-type wrench
Hard grass
10 x 12 x 14mm with a Y-type box wrench header
Y-type box wrench with a header 17 x 19 x 21mm
8 x 9 x 10mm with a Y-type box wrench header
Cross nut driver