Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Disposable Filter

Disposable Filter
Sales Price: 24.99 SGD
Review Rating: 4.62
8 Customer Reviews
5 star 6
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
塗料片付け
5
From Japan
On 2019-02-07 23:18:48
十分な強度で使用に問題なし。経済性も十分満足です。
This review is about item#283377.
Filtration of beeswax
5
From Japan
On 2018-11-27 19:32:45
I used it to filter molten beeswax. It was also possible to remove garbage with something like a spoon if it got clogged after filtration because it was quite resistant to heat.
This review is about item#283352.
Filtration of paint
3
From Japan
On 2018-08-13 15:58:47
Since the filter area is small, clogging tends to occur depending on the amount of dust and viscosity of the paint.
This review is about item#283352.
When painting
5
From Japan
On 2018-05-24 11:19:53
I use it without problems on the commodity. I will work if the price goes down a little more.
This review is about item#283352.
Filtration work
4
From Japan
On 2018-03-06 20:09:54
It was much more durable than I could imagine and it was possible to use it many times. If this is the case, since COSPA is better than the paper dispos, I will try to select it next time.
This review is about item#283395.
When filtering liquid
5
From Japan
On 2017-04-03 11:48:27
It is used when taking dust etc. in the liquid. It's strong and cost is cheap. I think I will repeat again.
This review is about item#283352.
When painting
5
From Japan
On 2017-01-25 14:52:53
It is good to sit alone on this, and it is also used for defoaming resin and others.
This review is about item#283395.
Filtration of organic synthesized polymer
5
From Japan
On 2015-09-29 16:04:56
I could not find another 200 mesh filter elsewhere and arrived at this product. Durability, smoothness of filtration, the bottom surface is on the cone and the bore size is reasonable, so it was smoothly transferred to the storage bottle. The main body is PP, the mesh is PEs, it is excellent in solvent resistance, it is very durable, it does not come out with garbage etc. It is very easy to wash, it can be used more than once. The structure is simple and very satisfied.
This review is about item#00283395.
1
Customer Who Viewed This Item Also Viewed
Cone Paint Strainer
Filter Funnel
Micro Strainer
Eco Mini Strainer
Multi Paint Strainer
Paint Filter Set
Oil filter network basket
Filter
Triangle filter
New Large Strainer
KOWA disposable filter 100 mesh
Strainer, No. 220