Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Expansion and contraction Tsutoka scissors shelf

Expansion and contraction Tsutoka scissors shelf
Sales Price: -
Review Rating: 4.00
1 Customer Reviews
5 star 0
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
I used it to organize my kitchen.
4
From Japan
On 2015-06-19 13:22:51
Since it slides to both sides, it can be installed at the exact size where you want to use, so it is easy to adjust to the length you want, so if you want to use it in a different place, you can move this item and it is reusable so it is very good I think it is a product. I felt that I was a little weak against the load that I was slightly dissatisfied. If you place a heavy thing on the shelf, the place to put double sided tape on the back side of the shelf will float. I was disappointed that it was a full mark if it was a product more resistant to loads.
This review is about item#05701824.
1
Customer Who Viewed This Item Also Viewed
SE pipe shelf
Pipe shelf S-type two-stage
Bumping stainless 2 Dantana
Two-stage hanging kitchen shelf
1-stage hanging kitchen shelf
Pipe rack A type two-stage
Pipe rack A type 1 stage