Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Tunnel Packer

Tunnel Packer
Sales Price: 2.99 SGD
Review Rating: 4.56
18 Customer Reviews
5 star 10
4 star 8
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 18 of 18 Reviews
At home garden etc.
5
From Japan
On 2018-10-20 16:11:23
Pittanko in the frame of the field, OK in the typhoon of the other day.
This review is about item#8466334.
Fixing of insecticidal net for agriculture
5
From Japan
On 2018-04-24 18:50:24
Insecticidal net can be fixed easily and firmly. I am glad that it is a bit cheaper but the work efficiency has increased considerably so it's a repeat decision.
This review is about item#8466352.
To the net holding of vegetable tunnel cultivation
5
From Japan
On 2018-04-13 20:32:48
Because it is a washing scissors type, detachment is very easy to do. It is a handy item that can be used any number of times.
This review is about item#8466325.
Cultivation of radish
4
From Japan
On 2018-04-06 09:37:21
The clamping force was a little weak, sometimes being blown by the wind.
This review is about item#8466334.
I use it for the cultivation of agricultural crops
4
From Japan
On 2018-02-09 14:10:32
Although I use various kinds from before purchasing with monotaro san, this product is easiest to use and durable It should be a little cheaper
This review is about item#8466325.
tunnel
4
From Japan
On 2018-02-07 15:06:24
It was so easy as it was easily stopped. It is a place to worry about how much I was concerned.
This review is about item#8466325.
It is easy to remove
4
From Japan
On 2017-12-16 19:03:48
I was not sure if it was easy to install, The ease of removal is definitely above the usual packer
This review is about item#8466325.
Insect net fastener
4
From Japan
On 2017-06-03 04:42:04
Easy to stop but perfect if there is a color that is inconspicuous (eg green) if you can.
This review is about item#08466352.
Seat fixing
5
From Japan
On 2017-03-17 17:01:31
Used when stretching a nonwoven fabric or vinyl sheet on a tunnel pillar, it is very convenient and convenient. If you use it well, you do not have to bury the hem of the seat, saving labor.
This review is about item#8466334.
Ventilation work of vinyl tunnel
5
From Japan
On 2017-03-02 19:24:02
Easy to work, as you can use without attaching power when attaching or removing. Even if a strong wind blows, it will not come off and I would like to continue using it.
This review is about item#8466343.
To stop the insect repellent sheet
5
From Japan
On 2016-12-27 19:22:46
Because it is a clip type it is very convenient and removable for installation.
This review is about item#8466352.
Used for insect net of Chinese cabbage and cabbage
5
From Japan
On 2016-08-14 18:37:36
Although it is slightly stiff at the time of installation, it is firmly fixed and can be removed smoothly and the cost is also low, so it is also used for cold weather of seedlings at the time of planting at the planting time and thermal insulation.
This review is about item#8466352.
Holding of insecticidal net.
4
From Japan
On 2016-05-05 17:30:22
It is easy to hold down and be tolerant of strong winds and satisfied.
This review is about item#08466352.
Nylon sheet stoppers for agricultural tunnels
4
From Japan
On 2016-04-27 20:36:48
When you remove it many times, it gets sweet and comes loose. At the end the inside breaks and it becomes useless. The place connecting the two will expire.
This review is about item#08466352.
Alternative to grape tunnel vinyl's eyelet
4
From Japan
On 2016-04-17 00:24:37
You can omit the repair of eyelets
This review is about item#08466334.
Killarin net stop
5
From Japan
On 2015-09-25 17:38:27
It is cheap and good to use! It is!
This review is about item#08466343.
Tunnel support
5
From Japan
On 2015-01-02 15:58:46
It is cheaper and stronger than chakorimushi. I will order this from next time.
This review is about item#08466298.
Farm work tunnel tension
5
From Japan
On 2014-12-16 13:54:08
Because it is used for work that is often opened and closed, it is best if you can open it and stop it like a clip. I stop now with feeling like pushing into the pillar, so it will crack when I repeat it many times.
This review is about item#08466334.
1
Customer Who Viewed This Item Also Viewed
Gardening Pole Vinyl Supporter
Garden cross band
Vegetable garden Short Packer
Tsugikko 16
Film tomail
New Sekisui Paul
Tunnel strut
Vegetable garden simple packer
Plant Clips
Color Clips
Tunnel strut round
Tunnel holding Packer
(Steel) harvest greens
Tunnel presser packer 11MM
Vegetable garden Packer 16
Tunnel strut