Customer Reviews of Holder type clip Clicks without magnet
|
Sales Price: 4.99 SGD
Review Rating:
![]() 8 Customer Reviews
|
|
---|
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Maintenance of motorcycle

From Japan
On 2018-08-31 11:59:31
There is no particular problem. I appreciate the correspondence as usual.
This review is about item#8429951.
Retention of laboratory instruments

From Japan
On 2017-12-27 14:38:48
It is very convenient to hold a small device such as cable, tube, hand light, camera etc. in the air.
This review is about item#8429951.
Signboard display

From Japan
On 2017-08-23 14:03:22
I am firm and easy to use, I'd like to order again.
This review is about item#8429881.
Fixing operation procedure manual

From Japan
On 2017-06-06 04:57:29
When doing various work, it is very useful when there is no space to put the paper on which you wrote the procedure etc. It is appreciated that you can check the document without moving the face, body, hand etc. because you can fix the document to the eye.
This review is about item#08429811.
Exhibition

From Japan
On 2016-03-10 15:49:31
We used several straight type 100 types and five joint type five joints. Since the joint is solid, a bit of caution is required when bending. For straight type, place your finger on the joint part and carefully bend it. You dislocate it if you do not care. One was broken arm. (You can continue to use by removing the broken arm and directly connecting the clips.) It seems that even if you treat the somewhat rough hands of the joint five-stroke type, force is dispersed to each joint, it will bend freely as I thought. Since both types are user-friendly as expected, I will repeat them.
This review is about item#08430003.
Put the document

From Japan
On 2016-03-02 17:51:20
I could not find it at a nearby stationery shop and I wanted it so much, so I'm happy! It is easy to use because it turns around.
This review is about item#08429967.
Used on the other side of the monitor of the notebook PC with the communication equipment attached from the USB via the USB cable (for increasing the reception sensitivity)

From Japan
On 2015-06-12 07:50:08
Because it was a little too big, I will purchase small one size around the next time.
This review is about item#08429951.
I hold the document during PC work.

From Japan
On 2013-10-25 19:33:39
I use multiple to PC work while watching multiple documents. It is useful.
This review is about item#08429827.
1