Buy more than* S$200* and get FREE SHIPPING
Note
Due to the maintenance, we will close our website on June/22/2019 2:00-2:30am JST.
All customers might not shop on our website during the time. Thank you.

Customer Reviews of VU Joint takeout socket

VU Joint takeout socket
Sales Price: 5.39 SGD
Review Rating: 4.67
6 Customer Reviews
5 star 5
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
For toilet bowl flange exchange
5
From Japan
On 2019-06-11 18:12:49
When replacing flanges due to a flange installation defect under the toilet bowl or aged deterioration, the VU pipe is cut at FL, which helps to add up.
This review is about item#16537176.
Raising the drainage basin
5
From Japan
On 2018-07-02 15:35:31
The carry-out socket type is not put in the home center etc., and the purchase with the monotaro is very handy.
This review is about item#16537133.
To connect pipes. . .
5
From Japan
On 2018-03-21 09:47:31
It was cheap and satisfying product. Thank you very much.
This review is about item#16537158.
Extension of VU tube
3
From Japan
On 2016-10-03 09:05:15
We could not work unless we had to cut existing VU 50 in maintenance work, but since the other part was the same size, we could extend it when we had to extend with the same diameter. Although it comes out from other manufacturers, it is a part that can be used without any problems.
This review is about item#16537158.
Used for piping remodeling work
5
From Japan
On 2016-06-15 20:19:51
It can be used very conveniently. When there is no fitting fee for fitting, it comes in handy as it enters the inner diameter of the tube.
This review is about item#16537158.
Exchange toilet
5
From Japan
On 2016-06-14 21:48:19
It is light and easy to use. I also want to purchase.
This review is about item#16537176.
1
Customer Who Viewed This Item Also Viewed
VU socket
Toilet Joint Nipple
CU Cide nipple
CU Cide nipple (short)
DV exchange socket
CU exchange Joint
VU Joint S socket
Nipple takeout for VU tube
ABS Pipe Connector