Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Easy digging device

Easy digging device
Sales Price: 88.99 SGD
Review Rating: 4.00
7 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
寒肥のため
5
From Japan
On 2019-02-22 20:25:22
バラや庭木の寒肥を与えるのに使います。 今まではスコップで掘っていて 結構な時間をとられていましたが 赤土の堅いところでも簡単に穴掘りができました。
This review is about item#16722423.
畑で、獣除け柵の支柱や野菜の支柱立てに活用
5
From Japan
On 2019-02-15 15:26:53
従来はてこ棒を使って穴をあけていたが、振り上げるとき棒が重いこと、又振り下ろす際、同じ位置に下すのに苦労をした。  本製品は、穴の位置決めは先端を刺すだけで決められる。又、穴掘りは長いハンドルのため楽に回すことができ、土が一緒に上がってくるので掘り穴がきれい開く。まだ試験的な作業しかしていないが、後日本格的に支柱立てをするのが楽しみ。
This review is about item#16722414.
When to stand upright
5
From Japan
On 2018-05-31 10:20:39
In the former pillar (486's single pipe) stand up, fixed 1 meter angle with 50 cm drive and van wire, this hole digger is easy to make well and a beautiful hole is excavated and a single pipe enters the stone and the ridge It does not crumble nearer, it can be easily fixed and work can be done smoothly It is very good thing.
This review is about item#16722414.
Application of fertilizer
5
From Japan
On 2018-03-15 22:38:49
I used a shovel or scoop to drill for fertilizer application, but this work was honest and painful with age. I saw a scene sculpting a hole for fishing on the lake frozen on TV. When this equipment is present, it is easy to dig hole to the ground, it searches on the site of Monotaro. I found "Easy Hole Digger" at Kobayashi Tool Manufacturing Co., Ltd., the price is reasonable, I bought it immediately and tried using it. As I thought, I was surprised that it was easy for Miramiru to eat well, to apply fertilizer easily, and to utilize it more quickly. I am surprised by the ruggedness of the welded part and the sharpness of the spiral blade and the side blade, after cleaning it is easy to rinse with water and even if wiped with an oil cloth after drying it is likely to last long. I am very satisfied with this.
This review is about item#16722423.
Used for wells and drilling
2
From Japan
On 2017-07-27 16:12:02
The material was weak and useless I regret that I can not use it
This review is about item#16722423.
Digging a pipe
5
From Japan
On 2017-05-28 16:45:16
Although it was working with hard soil, it was possible to dig a hole easily.
This review is about item#16722414.
Underwater piercing of fields
1
From Japan
On 2016-09-29 19:21:43
When used once, the tip got steeper. There is improvement
This review is about item#16722405.
1
Customer Who Viewed This Item Also Viewed
Tannneji Ring Auger, Handle
W Spiral Hole Digging
Twist Hand Weeder
Golden Zojirushi Hs Hole Digging
Green gardening strut hole digging device
Multi borer Long
N number self
Gardening Post Puller