Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of High-speed wood drill

High-speed wood drill
Sales Price: 9.99 SGD
Review Rating: 5.00
4 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Wood drilling
5
From Japan
On 2018-06-03 13:41:51
Sharpness lasts for a long time. I cut about 1,000 pieces in Red Cedar, but the sharpness did not fall so much.
This review is about item#21483744.
Drilling into hardwoods
5
From Japan
On 2017-04-07 07:05:05
With ordinary woodworking drills, it is easy for mecha to go out on the surface, ironwork drills are easy to clog the wood even if it is divided several times, the deep hole makes the resistance bigger and the sound goes out, irritating and drilling I was doing. This is because mecha does not occur at all, it is difficult to cause clogging of chips, and the resistance is reduced so that the sound is difficult to produce. Although it is a shape that can not be sharpened strongly, Zelkova has more than 800 holes of φ12 depth 5 cm, but it does not feel a sharp drop. As the price is cheap, it is already feeling it was taken by the former, so I would like to exchange it as soon as it feels a sharp drop. If it says strongly, you may not be able to demonstrate the true value unless you fix it with a drilling machine and use it. It might not be suitable for manual work.
This review is about item#21483753.
Cutting of cheeses
5
From Japan
On 2017-02-08 20:19:34
It is very sharp and lasts long. Also, when the blade enters, there is no turnover of the surroundings at all. Since the inside of the drill is recessed, the resistance is small, and the blade hardly holds heat. For that reason, even though even a simple chip discharge force, hardening of chips due to heat is suppressed, and there is almost no clogging in the groove. As it does not go digging like a woodworking drill, it is easy to stop in the middle. Since the price is never so expensive, it is better to buy a normal woodwork drill if you buy it.
Cutting of cheeses
5
From Japan
On 2017-02-08 13:03:46
It is very sharp and lasts long. Also, when the blade enters, there is no turnover of the surroundings at all. Since the inside of the drill is recessed, the resistance is small, and the blade hardly holds heat. For that reason, even though even a simple chip discharge force, hardening of chips due to heat is suppressed, and there is almost no clogging in the groove. As it does not go digging like a woodworking drill, it is easy to stop in the middle. Since the price is never so expensive, it is better to buy a normal woodwork drill if you buy it.
1
Customer Who Viewed This Item Also Viewed
Knife Golf Tool BK
Reel type neck strap
Center reamer 120
GS Millball
Cobalt Highs wood drill
Knife Golf Tool T
Woodworking high-speed shiitake awl